2020/01/21
ID: 2554

Compact with high flow rate

Versatile proportional solenoid valve VPWS from Festo

The proportional solenoid valve VPWS from Festo is the optimal choice for the safe and precise control of gas flows. It is a lightweight, compact 15 mm cartridge valve with a flow rate of up to 210 l/min at 2 bar. It is grease-free and oil-free and is suitable for oxygen, carbon dioxide, air, nitrous oxide or inert gases.

The proportional solenoid valve is ideal for applications in compact spaces, for example for mixing respiratory gases with oxygen in medical ventilators and anaesthesia systems. But it is also suitable for laparoscopes and colonoscopes, as well as other surgical instruments which are operated with compressed air.

 

In addition to being used in medical technology for the safe and precise control of gas flows, the valve is used in applications with high demands in terms of cleanliness, such as the electronics and semiconductor industries or the dispensing and filling of protective gas in food production.

Festo is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. Festo has set standards in industrial automation technology and technical education ever since its establishment, thereby making a contribution to sustainable development of the environment, the economy and society. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. Digitalization, AI and the LifeTech sector with medical technology and laboratory automation are becoming increasingly important. The products and services are available in 176 countries. With about 20,800 employees in over 250 branch offices in around 60 countries worldwide, Festo achieved a turnover of around €3.81 billion in 2022. Each year around 7% of this turnover is invested in research and development. In this learning company, 1.5 % of turnover is invested in basic and further training. Festo Didactic SE is a leading provider of technical education and training and offers its customers worldwide comprehensive digital and physical learning solutions in the industrial environment.

© Festo SE & Co. KG
VPWS proportional valve
Safe and precise control of gases with the proportional valve VPWS from Festo.

Global Contact Person

Downloads

Share Press Release