Degassing and sealing are core processes in battery cell production that directly follow the initial contacting of the battery cells with electrical voltage. The battery cells are pierced with lances and the forming gas produced during contacting is extracted. Pneumatic and electric actuators from Festo are used to handle and pierce the battery cells. Read press release Image Festo SE & Co. KG 06/01/2026 | Global Reliable degassing in battery cell production Degassing and sealing are core processes in battery cell production that directly follow the initial ... Read press release
Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past: Liebherr has developed a system that automatically removes the battery cover screws - regardless of whether they are attached horizontally or vertically to the battery housing. The CMAD servo-pneumatic position controller from Festo, which makes position-independent unscrewing possible in the first place, plays a major role in this automation solution. Read press release Image Festo SE & Co. KG 05/29/2026 | Global Automated dismantling of electric batteries Manual disassembly of end-of-life batteries in electric vehicles is now a thing of the past ... Read press release
The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year until 2030. At the same time, the production processes for the electrified powertrain are changing. While semi-automated production processes have dominated traditional automotive manufacturing with combustion engines up to now, the manufacture of battery cells and electric motors is increasingly developing into fully automated production processes. As a leading manufacturer of automation technology, Festo has the right solutions for this along the... Read press release Image Festo SE & Co. KG 05/29/2026 | Global Everything under control from battery cells to ... The number of vehicles with electric drives worldwide is forecast to grow by around 30% per year ... Read press release
Experts estimate that around 3 million tons of used batteries from electric cars will be due for recycling in 2030. This inevitably raises the question of sustainability, as batteries are energy storage devices made from critical raw materials. Festo therefore not only offers modular automation concepts for cell production, the assembly of battery modules and packs and for platform integration, but also for dismantling and recycling or separating the materials. Read press release Image Festo SE & Co. KG 05/29/2026 | Global Automated processes for battery recycling Experts estimate that around 3 million tons of used batteries from electric cars will be due for ... Read press release
05/29/2026 | Global The Battery Show Europe 2026 Visit Festo at the Stuttgart trade fair in hall 3 at stand E10 Press Releases (4) Images (16) View press kit Image Festo SE & Co. KG
2024/05/28 | Global Battery Show Europe 2024 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Press Releases (4) Images (15) View press kit Image Festo SE & Co. KG
2023/05/22 | Global Battery Show Europe 2023 Reliable, economical, sustainable: The circular battery life cycle – solutions from cell production right up to ... Press Releases (5) Images (17) View press kit Image Festo SE & Co. KG
2022/06/23 | Global Battery Show Europe 2022 28 to 30 June, 2022 Press Releases (3) Images (9) View press kit Image Festo SE & Co. KG