25 per cent less power consumption
Energy savings of 25 per cent and more in compressed air systems for machines and systems – often it’s the small actions that make the difference, such as reducing the pressure level, detecting leakages or shortening tube lengths. With the Compressed Air Energy Efficiency PreAudit, Festo is opening up enormous saving potentials for system operators throughout their entire compressed air system.
More and more system operators want to increase the energy efficiency, and thus the performance of their compressed air systems. Many also recognise the need to implement the global standard ISO 50001 for systematic energy management in their plants. Operators in Germany, for example, can benefit from partial exemptions through the EEG reallocation charge (EEG = German Renewable Energy Sources Act) and tax relief on electricity and energy.
Quick wins through quick checks
So where’s the best place to start? Where can you get the quick wins? This is where a kind of quick check comes in. In the PreAudit, all parts of a compressed air system are subjected to a point-by-point analysis. With the PreAudit from Festo, system operators can detect weaknesses immediately and know for certain which measures are most likely to work for their compressed air system.
During the PreAudit, the energy experts from Festo examine the compressed air generation and preparation, assess the compressor utilisation, analyse the compressed air quality and measure the pressure drop in the system. In the quick check, the specialists carry out a representative leakage detection test on selected systems and also check that the pneumatic components of these machines are used in an energy-efficient way. The customers get a detailed report with accurately documented data and recommendations for action weighted by priority. The documentation sets out the CO2 emission values that many companies need to state in their sustainability report in accordance with GRI or GHG for example.
Fully integrated approach
Only a few providers are in a position to assess the entire compressed air system. Frequently, the focus is solely on compressed air generation. With its Compressed Air Energy Efficiency PreAudit, Festo is pursuing an integrated approach – from generation to application – and has gained extensive experience over the last five years.
The PreAudit forms part of the comprehensive Festo Energy Saving Services range, which is certified to DIN EN ISO 11011. This requires Festo’s auditors to complete extensive training. 16 auditors are now qualified to carry out the Compressed Air Energy Efficiency PreAudit of machines and systems on-site for customers around the world.
费斯托 (Festo)是一家全球性的独立的家族企业,总部位于德国埃斯林根。自成立以来,Festo在工业自动化技术和技术教育方面制定标准,从而为环境、经济和社会的可持续发展做出贡献。公司为超过35个行业的30万家工厂和过程自动化客户提供气动和电驱动自动化技术解决方案,其中生命科学和实验室自动化业务受到越来越多的关注。Festo产品和服务遍布176个国家。2022年,费斯托在全球61个国家的250多个分支机构拥有约20800名员工,实现销售额38.1亿欧元。每年约7%的销售额用于研发。在这家学习型企业,1.5%的销售额用于基础和进一步培训。Festo 教学培训 (Didactic SE) 是全球领先的技术教育和培训供应商,为全球客户提供工业环境中全面的数字化和常规学习解决方案。